Toshiba Motif

Welcome to the Toshiba Storage Blog

Discussing the latest in Storage solutions

The Advantages of Toshiba's Helium-Sealed HDDs: Unleashing Efficiency and Capacity

In the fast-paced realm of data storage, innovation is paramount to meet the escalating need for greater capacity and enhanced performance. One such technological leap comes in the form of Toshiba's helium-sealed hard disk drives (HDDs), a game-changer that offers significant advantages over traditional air-filled HDDs.

Helium, a noble gas, holds the secret to unlocking greater efficiency in data storage. Being smaller than air molecules, helium reduces aerodynamic drag within the HDD, resulting in less turbulence and buffeting of the rotating disks and head suspension assemblies. This reduction in turbulence has a domino effect on other performance aspects.

One of the major benefits is improved positioning precision. With less vibration and wobbling at high RPM, the actuator arms can achieve higher accuracy in reading and writing data, increasing the areal density that can be achieved on the platters. Consequently, the helium-sealed HDD can accommodate more data in the same form-factor, leading to higher storage capacities within the industry-standard 1-inch form-factor. Moreover, the reduced turbulence allows for the utilization of nine disks within the HDD, contributing to the enhanced storage capacity. By reducing the distance between platters, the overall data density is maximized without compromising reliability. Helium's unique properties also make it easier to maintain an optimum "fly height" for the recording head above the platter surface. This controlled "flying" of the head ensures accurate data reading and writing. Additionally, the lower drag force experienced by the spinning platters in helium-sealed HDDs results in significant energy savings. Compared to conventional air-filled HDDs, Toshiba's helium-sealed MG08 series HDD consumes approximately 50% less power per gigabyte (W/GB)*2, making it a more eco-friendly and cost-effective choice for Cloud-scale data centers using a large number of HDDs.

In conclusion, Toshiba's helium-sealed HDD represents a leap forward in data storage technology, providing higher capacity, improved performance, and energy efficiency. By harnessing the advantages of helium, Toshiba continues to push the boundaries of innovation and offers a reliable solution for today's data-intensive world.

Disclaimer
The views and opinions expressed in this blog are those of the author(s) and do not necessarily reflect those of Toshiba America Electronic Components, Inc.

Comments are closed
A new window will open