It has been reported that there may be default password vulnerability in the CANVIO (STOR.E) wireless products.
Please be sure to change the default password upon your initial use of the CANVIO (STOR.E). If you do not change the default password there is a possibility that an unknown person may utilize the wireless communications range of the CANVIO (STOR.E) and may access the entire shared file system.
Product Name
(varied at location) |
Model No. |
Product
image |
vulnerability |
Canvio AeroCast /
Canvio AeroCast wireless HDD |
HDTU110*KWC1 |
 |
Default Password |
Canvio Wireless Adapter /
STORE.E Wireless Adapter /
Canvio CAST Wireless Adapter |
HDWW100*KW*1 |
 |
Null Default Password |
| Model No. |
Threats |
| HDTU110*KWC1 |
An unknown person within the wireless communications range of an affected product with knowledge of the default password may access the entire shared file system in the product without restriction.
|
| HDWW100*KW*1 |
An unknown party within the wireless communications range of an affected product may access the entire shared file system in the product without restriction.
|
Change or set the password
Immediately change and replace the default password upon first usage of the product with a sufficiently strong and unique password.
See US-CERT Security Tip ST04-002 and Password Security, Protection, and Management for more information on password security.
Counter measure for each model:
| Model No. |
Countermeasure |
| HDTU110*KWC1 |
Please be sure to change the default password immediately upon first usage of the product. To set your unique password, please refer to this user manual and the FAQs on your applicable regional support site.
The default password is automatically set upon shipping of the product. Even if the default password is changed to your unique password, your unique password may be reset to a default password in the following situations:
- When the user resets the product by using the associated App or by depressing the Reset button to accomplish a reset.
- When the option “Enable factory default after firmware upgrade” is selected and the user updates the firmware.
|
| HDWW100*KW*1 |
Please be sure to enable and set your unique password immediately upon first usage of the product. To set your unique password, please refer to this user manual and the FAQs on your applicable regional support site.
The default password is null upon shipping of the product. Even if your unique password is set, your unique password will be reset in the following situations:
- When the user resets the product by using the associated App or by depressing the Reset button to accomplish a reset.
- When the option “Enable factory default after firmware upgrade” is selected and the user updates the firmware.
|
References
Alert (TA13-175A) Risks of Default Passwords on the Internet
- Revision History
-
Feb. 28 2018 Date revision published.
Contact Information
Please visit the following website and choose the applicable Consumer Storage Solutions website for your region.
Toshiba Storage