Toshiba Announces Volume Availability of 8TB HDD Model - Company's Largest Enterprise Capacity HDD

Latest Toshiba 3.5 inch Enterprise Capacity 8TB1 SATA HDD achieves volume shipment status

April 5, 2017

MG05_tmb

IRVINE, Calif. — Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, announces volume availability of its next MG Series HDD – the MG05ACA800 – providing 8TB for business critical servers and shared storage systems. With a 33 percent increase in capacity from the previous 6TB SATA generation, this drive is the first Toshiba 8TB SATA 6.0Gbit/s2 capacity-optimized storage for the enterprise, making it the largest capacity ever produced by Toshiba. The drive improves sustained transfer rate performance by 12 percent when compared to the MG04ACA.

The new 8TB model can help to improve the operational efficiency of storage infrastructure by increasing the capacity available in the industry-standard 26.1mm high form-factor. The drive’s high capacity SATA interface and performance characteristics match-up well with requirements for applications such as software-defined storage infrastructures, public and private cloud deployments, digital archives and disk-based backup and data protection solutions.

The drive’s power management features help to optimize operating costs and operating environments during off-peak activity periods. The 8TB SATA HDD is designed for 24x7 operation and provides a 550TB transferred-per-year rated workload3, with a 2,000,000-hour MTTF4 rating. Additionally, this is the first Toshiba Enterprise capacity SATA model to support the new industry-standard host-initiated power-disable feature for improved device management capability.

“Accommodating rapid data growth continues to be a prime focus for both cloud-scale and on premise IT environments,” said Scott Wright, director of HDD marketing at Toshiba America Electronic Components, Inc. “Toshiba’s new 8TB SATA enterprise-capacity HDD provides high capacity per-spindle. This helps OEMs and cloud service providers (CSPs) deliver enterprise-class storage capacity for business critical workloads that need to keep pace with rapid data growth.”

As was recently announced, new IDC market report5 identified Toshiba as the fastest growing HDD vendor segment in 2016 over 2015, as measured by revenue and units. Toshiba’s growth was aided by their comprehensive array of innovative HDD model offerings across different primary market segments. The new 8TB SATA HDD, part of the MG Series, is aimed at Enterprise Capacity and Data Center needs.

In February 2017, our cumulative Near-Line Enterprise HDD production number reached 10,000,000 units. The MG Series HDDs, which are Near-Line Enterprise HDDs, are sampling today to OEMs and Systems Integrators. Typical use cases include tiered storage infrastructure for public and private cloud deployments; virtual desktop interface (VDI); email servers, data-protection and other business-critical systems use-cases; public and private cloud storage; software defined storage; business critical servers; business critical storage systems (including NAS and SAN); disk-based backup systems (including cloud-scale data protection); data archives and digital records storage; and SMB servers and storage platforms.

For more information on Toshiba’s line of storage product, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba’s storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and follow @ToshibaStorage on Twitter.

About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide. Visit Toshiba's web site at http://toshiba.semicon-storage.com.

1Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary

2Read and write speed may vary depending on the host device, read and write conditions, and file size.

3HDDs keep track of various drive usage such as power on hours, lifetime writes and lifetime reads from the host computer.  

With this data we calculate an Annualized Workload Rate, under 40 deg. C ambient environments, Annualized Workload Rate = (Lifetime Writes + Lifetime Reads) * (8760 / Lifetime Power On Hours) in case Power On time is 8760h or longer. Otherwise (i.e. Power On time is shorter than 8760h),

Annualized Workload Rate = (Lifetime Writes + Lifetime Reads)

Each drive is designed to perform up to the Annualized Workload Rate stated, after which the drive may be expected to decline. The Annualized Workload Rate in no way alters the warranty policy for such drive.

4MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF 

5Fastest growing HDD vendor in 2016 over 2015 as measured by revenue and units based on IDC Worldwide 4Q16 HDD Shipment Results and Four-Quarter Forecast Update (Feb 2017 - Doc #US42306617)

 

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

will open in a new window Will open in a new window.
to top To Top