Toshiba Storage Products Milestones
- 2009 – Toshiba acquires
Fujitsu HDD business, creating the broadest portfolio of products in the
storage industry
- 2009 – Adds complete
system backup and password-protected encryption to personal storage line
- 2009 – Adds 500GB USB
2.0 portable external hard disk drive (HDD) to personal storage line
- 2008 – Brings SATA technology
to automotive HDDs with 80GB model
- 2008 – Introduces 250GB
1.8-inch Micro SATA HDD for computing applications
- 2008 – Announces 240GB
1.8-inch PATA HDD for compact consumer electronic and computing applications
- 2008 – Launches highest
capacity 2.5-inch HDD - 400GB
- 2008 – Commences production
of reduced halogen and other potentially hazardous substances with its
160GB/platter 5400 RPM 2.5-inch series
- 2008 – Debuts series
of third-generation high-performance 2.5-inch 7200 RPM HDDs
- 2008 – Ships slim 160GB
1.8-inch 5400 RPM Micro-SATA HDD
- 2008 – Brings highest
capacity portable external hard drive to market with 320GB USB 2.0-enabled
solution
- 2008 – Ships first 6Gb/s
Serial Attached SCSI (SAS) enterprise HDDs*
- 2008 – First HDD manufacturer
to meet the OPAL encryption specification*
- 2007 – Introduces the
industry's first 300GB 2.5-inch external HDD*
- 2007 – Launches the
first 15K 2.5–inch HDD with SAS interface*
- 2007 – Achieves highest
areal density demonstration at one terabit per inch using patterned media*
- 2007 – Offers first
1.8-inch HDD with CE-ATA interface.
- 2007 – Enters personal
storage market with a line of portable USB 2.0 external hard drives
- 2006 – Leads market
with 200GB 2.5-inch 5400 RPM HDD
- 2006 – Extends perpendicular
magnetic recording (PMR) reach to 0.85-inch and 2.5-inch HDD offerings
- 2005 – Expands engineering
expertise with acquisition of Matsushita's U.S.-based HDD Design Division
- 2005 – Ships 100 millionth
HDD
- 2005 – First to commercialize
PMR, achieving 133 gigabits per square inch on 1.8-inch HDD
- 2004 – Recognized in
the Guinness World Records™ for world's smallest HDD (0.85-inch)
- 2004 – Announced world's
first 2.5-inch SAS Enterprise HDD*
- 2003 – Introduces the
world's first 2.5-inch SATA HDD*
- 2002 – Introduces U320
SCSI drive*
- 2001 – Starts utilizing
environmentally sound printed circuit board assemblies (PCBA) in all new
HDD products
- 2001 – Commences volume
production of first HDD designed for automotive applications
- 2000 – Debuts the first
high-volume 1.8-inch HDD, igniting the start of the digital music revolution
- 2000 – Breaks the areal
density world record with 56 gigabits per square inch*
- 1999 – Introduces U160
SCSI drive*
- 1999 – Leads the areal
density race by breaking the 20 gigabits per square inch barrier*
- 1998 – First manufacturer
to transition to GMR across its product line*
- 1998 – Introduces first
HDD to utilize giant magneto resistive (GMR) recording head technology
to achieve 2.16GB on one 2.5-inch disk
- 1991 – First 2.5" HDD,
90MB*
- 1990 – Ships first HDD
using glass media on a single-platter, 40MB 2.5-inch hard drive
- 1989 – Establishes voluntary
social and environmental program aimed for the betterment of humans worldwide
and the health of the planet
- 1986 – First 3.5" HDD,
26MB*
- 1983 – First 5.25" Disk
Drive, 27MB*
- 1981 – First 8" Disk
Drive, 48MB*
- 1980 – Establishes industry
leadership with the world's first 10.5-inch HDD and begins the Eagle product
line*
- 1969 – Delivers first
Hard Disk Drive, 14" Form Factor*
- 1967 – Enters the HDD
industry with 14-inch HDDs
* Milestone achieved by acquisition.